4/29/2016 12:34 PM | |
Joined: 3/17/2015 Last visit: 2/23/2024 Posts: 9 Rating: (1) |
Good morning, this morning this issue happen also to me. I have tryd to do the what you describe below but without any result. I'm using TIA V13 sp1 and i cannot go online, the only interface present is teleservice. If i open PG/PC interface, this is totally empty. Any other suggestion? Thanks in advance Simo ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/29/2016 12:37:03 PMNew subject after splitting |
|
4/29/2016 1:34 PM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
Dear sibo Please check the check box available at the ethernet card at set pg/pc ---> LLDP/DCP if not checked then do it and same with the PNIO adaptor the another thing you can check is the interface add/remove try to add the drivers and if feeling problems then post it also post the snapshots |
Thanks and Regards |
|
4/29/2016 1:44 PM | |
Joined: 3/17/2015 Last visit: 2/23/2024 Posts: 9 Rating: (1) |
Dear Christoph, i have already do what you suggested without any result. Thanks |
4/29/2016 2:04 PM | |
Joined: 3/17/2015 Last visit: 2/23/2024 Posts: 9 Rating: (1) |
Here we are. Thanks Attachments7epaImp64x_2016-04-29.13.50.42.txt (2090 Downloads) |
4/29/2016 2:23 PM | |
Joined: 3/17/2015 Last visit: 2/23/2024 Posts: 9 Rating: (1) |
I've done, but nothing changes. |
Follow us on