4/4/2019 9:59 AM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hello ronaldo7, have you published the data on the web server? You have to stored all pictures and required scripts on the Web server to enable them to be displayed or run on the Web client. All screens and scripts must be prepared accordingly. The Web View Publisher is used for this purpose. More Information about the Web View Publisher you can find in the manual "PCS 7 Web Option for OS" in section "How to publish data". With regards |
This contribution was helpful to
1 thankful Users |
4/4/2019 3:47 PM | |
Joined: 9/9/2015 Last visit: 9/28/2025 Posts: 732 Rating:
|
Dear ronaldo7, Let me try to help you. I would assume your webserver is setup by using OSC , WinCC application Client. Are you able to open the runtime locally in the webserver and showing no error? (If yes, can you take a screenshot?) Have you assign server data in your Webserver OS Client in the simatic manager? Right click the webserver/OSC in the configuration-> Assign server data. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
4/5/2019 5:39 AM | |
Joined: 9/9/2015 Last visit: 9/28/2025 Posts: 732 Rating:
|
Dear ronaldo7, Just to extend the capability of your web client, you could try to run an exe: <Program Files>\Siemens\WinCC\Webnavigator\Client\bin\WinCCViewerRT.exe This is to open the WinCC runtime in web client in the standard window interface. (At the Web Client Station). The look and feel will be the same with OS Client and the window size will be bigger as compared to the one with internet explorer, the web version. After your first setup/double click on the exe, an XML file that record the information will be stored at "YourUserFolder" -> AppData-> LocalLow-> Siemens-> SIMATIC.WinCC-> WebNavigator-> Client -> WinCCViewerRT.xml (you may access it by key in %TEMP% into your Folder directories) If you delete the xml file, once you click the WinCC ViewerRT.exe, a dialog box will be popped out to request for Server Address and Credentials. You can insert the address and default username/password into the xml file for quick access. For further information, you may refer to the web option manual -> Search WinCCViewer. (FYI, the xml file related guide is not written in the manual. ) Hope it is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
Follow us on