6/26/2009 9:13 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, Just as an info. Siemens has a DVD with Technical Product Data for CAx Applications . Among other info, there are pictures in DWG format. More details here http://support.automation.siemens.com/WW/view/en/34066427 |
Best regards |
|
6/26/2009 10:11 PM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
I did not find the picture which i am looking for on the above link, where can I download DVD from? |
6/27/2009 1:32 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Lalit, Nice to replyto one ofyour threads again. the CAX DVD is not for free. However, the details you are looking forcan be found on manuals. For S7-300 systems, there are some good manuals that you should always have with you. 1 - SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications. To know where the Profinet port is located for CPU 315-2 PN/DP, please look at page 27. 2- SIMATIC S7-300 CPU 31xC and CPU 31x: Installation. 3- S7-300 Instruction List. 4- SIMATIC S7-300 S7-300 Module data. (I think you already have this one) In chapter 8, you will find all information regarding IM365. IM365 modules (Send/Receive)come with permanently connected cable(1m). So, there is no connectors. IM365 modules don't have DIP switches. For the CP341, Please look at chapter B (Connecting cables) in themanual. There's also a manual for Modbus slave driver. I hope you will find it useful. Best regards. H-H |
This contribution was helpful to1 thankful Users |
6/29/2009 3:14 AM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Hi H-H, Thanks for the info, I am still unable to find the info about IM-365 modules, I mean how those will be connected together, will that be a connector cable or we would need to wire it, how big the size of the connector, if you have those details, please reply.
|
6/29/2009 7:04 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Lalit, The IM365 modules come preassembled. There's no connector. The cable is permanently connected so you can't take it out of any module. From S7-300 Module Data (Page 404), 8.4 Interface module IM 365; (6ES7 365-0BA01-0AA0) Special features of interface module IM 365: ● Preassembled pair of modules for rack 0 and rack 1 ● Total power supply of 1.2 A, of which up to 0.8 A may be used per rack. ● Connecting cable with a length of 1 m already permanently connected. Best regards. |
This contribution was helpful to1 thankful Users |
6/29/2009 9:21 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello Lalit, Here's a pictures of the IM356. When you will order it, you will recieve one package contans two modules (send) & (Recieve) modules with 1meter cable connected between them. Dimension of each module is WxHxD = 40x125x120 mm. Hope this info will help you. AttachmentIM pictures.zip (148 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
6/29/2009 4:42 PM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Thanks guys, I am fairly clear about, CPU & IM365 Modules, and I found the pin configuration of CP341, however I still did not find the modubus slave picture, how will it be connected to CP341, if some one of you has the picture of CP341- with the modbus slave driver please do post here. |
6/29/2009 5:28 PM | |
Posts: 261 Rating: (42) |
Hi lalit, If you already loaded the modbus master setup you can find the information under the Modbus Master pdf. The path is Start>simatic>documentation>English |
6/29/2009 7:32 PM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Still Can't find any picture how CP341 and dongle combination will look like.. |
6/29/2009 11:59 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Lalit, I couldn't find a picture showing what you want. All I could find is how to install the dongle from the manual(Page17). Installation Introduction In order to use the CP with loadable drivers, you require a dongle. When the dongle is plugged in, drivers can be loaded. For the CP 441-2, you can download drivers for both interfaces. Inserting the Dongle To insert the dongle, you must remove the CP from the rack. The module slot where you insert the dongle is located on the back of the CP above the plug-in connector for the backplane bus. |
Last edited by: H-H at: 6/30/2009 12:00 AM |
|
6/30/2009 7:31 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hi, This night I'll send you (PM) "pictures" for this modules extracted from http://support.automation.siemens.com/WW/view/en/34066427 Just to close the thread. Regards Hristo Mihalev |
6/30/2009 8:04 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, Here's the *.dxf file of CP341.. Extracted from http://www2.sea.siemens.com/Products/Automation/CAD Regards, Attachment6es73411ch010ae0_001_all.zip (110 Downloads) |
Last edited by: Ayman Elotaify at: 6/30/2009 8:07 AMAyman Elotaify |
|
6/30/2009 9:23 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hi, Perhaps you can find some pictures here: Bilddatenbank Best regards, Wizard |
6/30/2009 2:09 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Dear all, I thought (still think) Lalit is able to write the part number of the CP in this site's home page and see the picture of the module. I think he just wanted to know how the dongle looks like and how both CP and dongle together will look like.
Anyhow, I'm reallyglad since we all just aim to help each other. I've foundthe attachedpictures for both dongle and CP (rear view) on Ebay and I hope Lalit will find them useful. Lalit, One last thing, This part number is for an old CP. Please take a look at this. Best regards. H-H AttachmentCP 341 with dongle.zip (145 Downloads) |
This contribution was helpful to3 thankful Users |
6/30/2009 8:14 PM | |
Joined: 12/20/2008 Last visit: 8/25/2022 Posts: 556 Rating: (236) |
Thanks, I found it. Lalit |
Follow us on