12/29/2011 11:47 AM | |
Joined: 1/28/2009 Last visit: 3/14/2024 Posts: 6836 Rating: (1358)
|
Dear PilotPM, "PID Self Tuner" package is intended to help automation engineers to evaluate process model and use optimized PI or PID parameters. You can find the range of product here: http://support.automation.siemens.com/WW/view/en/10805417/133200 and the manuals here: http://support.automation.siemens.com/WW/view/en/10805417/133300 and sample examples here: PID Self Tuner: Example Adapted to Standard PID Control V5.1 Please read the manual carefully before even ordering the product.It is not really difficult to use but it is really tricky. If you follow the provided samples,CPU set the Tuner to manual. For the first optimization you set "Man_on" to "False" and "Adapt1st" to "True".Select proper set point and wait until the set point reached and analyze the parameters if they are satisfactory.Further optimization is possible by using "Adapt_on". Hope this helps Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 5/7/2013 10:18 AM// typo |
|
This contribution was helpful to1 thankful Users |
5/27/2014 5:21 PM | |
Posts: 15 Rating: (0) |
There is only simatic tool? I do not use TIA in the industry where I work |
5/27/2014 6:24 PM | |
Joined: 1/28/2009 Last visit: 3/14/2024 Posts: 6836 Rating: (1358)
|
Please , read more in Page#5 of the following manual.STEP 7 > 3.2 as the requirement of using this package is definetly a part of SIMATIC Manager (like the latest STEP 7 V5.5).Contact your SIEMENS local representative for more help regarding the product! PID Self-Tuner V5
|
Last edited by: hdhosseini at: 5/27/2014 6:26 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on