5/12/2018 2:00 PM | |
Posts: 64 Rating: (0) |
Hello all: We have Pipe Mill Machine. We use flyingsaw system with Simotion D425 integrated Sinamics. We have problem with synchronous between External Encoder and Carriage Axis when various speed change (+) or (-) suddenly . For example : if machine speed 30 meter/min change suddenly to 60 m/min , big difference in tube length. if machine speed 60 meter/min change suddenly to 0 , we get on some problems as shown in attached file. AttachmentPipe Mill Machine problem.docx (81 Downloads) |
5/14/2018 6:27 PM | |
Posts: 125 Rating: (11) |
The censor filter makes my last post seem more profane. It's censoring a 5-letter word for "wasted material". |
Follow us on