12/29/2010 2:45 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
How and for which analog measurements can you use the function FC105 "SCALE" to convert the integer values (INT) into real number values? and go to FC106 analogical... |
12/29/2010 2:53 PM | |
Posts: 19 Rating: (0) |
ok i will try it but need i to scale it first (fc 105) |
12/29/2010 3:56 PM | |
Posts: 19 Rating: (0) |
thnx it works but 1 question if i want to scale it to is my input then piw 272? and why is hi_lim not 10? because the max is 10V |