11/2/2018 4:05 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi Alexander, Do you have the PCS7 trial license installed? Maybe this is interfering with the other licenses. You do not need a license for PKZIP so that is correct. Which licenses do you have installed? and which PCS7 version do you have? |
If I could help you, you can use the RATE button. Thank you. |
|
11/2/2018 9:13 PM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
Thank you for the response. I will check Monday if The trial License is installed and i will revert back. |
11/5/2018 4:22 PM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
There are two PCS7 Trial License found in the ALM. See attached Picture. We are running PCS7 V8.0. |
11/5/2018 6:34 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, you can remove the trial licenses. If your not sure, transfer the trial licenses to a USB stick so you have them still available. |
If I could help you, you can use the RATE button. Thank you. |
|
11/7/2018 12:13 PM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
I have the Trial License removed and PKZIP reinstalled but no difference. It is still asking for the key. |
Follow us on