4/26/2016 9:31 AM | |
Joined: 5/20/2015 Last visit: 4/12/2024 Posts: 215 Rating: (3) |
hi guys Please suggest me PLC and I/o's for the following requirments: 1)DI- 88 2)DO- 48 3)AI- 16 along with 8 RTD channel With 4 PID. 4)AQ- 4 it is Stand alone Pharma Industries project on WinCC 7.3 SCADA system along with the Audit trail and reporting. Software Side system is finalized. please Suggest Cost effective PLC and IO modules which can give satisfying output. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/26/2016 1:12:53 PMNew subject after splitting Let's do it... |
|
4/26/2016 2:53 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi gabbar For a basic I/Os with no special function as high speed or counters just 24 VDC and without taking in consideration field communication bus or any unmentioned data, check the attached file. You can also download SIMATIC Selection Tool http://www.siemens.com/tia-selection-tool
AttachmentBasic Configuration.xlsx (166 Downloads) |
Best Regards |
|
This contribution was helpful to3 thankful Users |
4/27/2016 5:54 AM | |
Joined: 10/17/2007 Last visit: 4/19/2024 Posts: 3969 Rating: (340) |
Why do you NOT post this thread in "SIMATIC S7--HARDWARE" branch?
|
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
4/28/2016 10:08 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
hi, use IM 151-7 CPU and add no. of DI/DO/AI/AO module with required specification up to 64 ,it looks better solution with low cost as it has intergrated profinet port. Viral patel |
This contribution was helpful to1 thankful Users |
4/28/2016 10:46 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, I believe that this thread will be too long. Before start to select the optimum solution for an application, there are many question you have to answer.
Finally, As I told, You will recieve here many answers with many configurations, If you answered the above questions, you would have just few solutions for your application. Then, select the lowest price. And also take care that the price of a project is not only price of modules and CPU, but also take into consideration accessories price, panels, software packages compatible with your hardware, ...etc. Hope this helps. |
Ayman Elotaify |
|
4/28/2016 10:59 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi gabbar, In my opinion, no one of us can give you a suitable solution for your project, only by knowing how many inputs and outputs are needed. There is much more to know to give you the rigth solution. I think you can´t get this solution in a forum. If I were you, I would contact the technical consulting/engineering support of local Siemens representation. Have a look in contact database hope this helps, regards, |
FCK WAR! |
|
Follow us on