11/30/2015 6:18 AM | |
Posts: 1 Rating: (0) |
Dear sir, I need help to take PLC back up On 810D. I am using step 7 manager version 5.5 & USB A2 adaptor. when i start upload station to PG it is giving message unknoen cpu type. can you please attach the procedure file for backup/restore using USB A2 Regards, Sachin harne ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2015 3:03:34 PMNew subject after splitting |
|
12/1/2015 9:55 PM | |
Joined: 10/17/2007 Last visit: 5/11/2024 Posts: 3985 Rating: (342) |
Try to only back up "S7 Program" NOT uploade station to PG. I think the problem is not communication--(you ask for USB A2) --the problem is the PG or PC with SIMATIC Manager you use is a standard while PLC CPU in 810D is special type of CPU. If you want back up the whole --that means including HW configuration --you need install SINUMERIK ADD-ON files to your PG, which need purchase from Siemens , including in the CD_ROM NAMED "SINUMERIK TOOL BOX"
|
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
Follow us on