4/22/2021 2:19 PM | |
Joined: 3/2/2017 Last visit: 9/20/2024 Posts: 88 Rating: (3) |
Hi I am Using s7-1214F PLC and controlling G120C and V90 drivers. I am using TIA Portal V15.1 and GSDML-V2.32-Sinamics_V90PN-20190415 with SINA_POS block to drive V90. But When I power up the machine it doesn't go in to RUN mode as I selected from PLC's properties (Startup mode Run). When I check diagnostics buffer I says "potential inhibit/break reason for next startup". How can I solve this? Diagnostics image are in attechments. Thank you. I cannot add more than 1 attachment :( [snip] AttachmentScreenshots.zip (247 Downloads) |
Last edited by: Ufuk1985 at: 04/22/2021 14:22:28Last edited by: Jen_Moderator at: 04/23/2021 07:02:31Removed links and added files as an attachment. |
|
4/22/2021 3:38 PM | |
Joined: 3/2/2017 Last visit: 9/20/2024 Posts: 88 Rating: (3) |
Solved it thank you. If I select correct version(HSP) It doesn't work with s7-1200 on TIA V15.1. I have to use GSD |