2/11/2011 5:22 PM | |
Posts: 259 Rating: (5) |
Hi, I make backup form some old machine with Sinumerik 810T. I have ASM, TEA1, TEA2, RPA1, TOA, ZOA1, all programs and PCP file. Unfortunately i couldn't find PCA (PLC alarm text). I think this file is deleted on the machine because in diagnose mode you can see only number without any description. And my question... it is some way to open in STEP5 or in other program PCP data that I have from backup. I need to understand PLC code to make new PCA with description, and most important to know what cause this alarms.Any advice would be appreciated... With regards, makaveli AttachmentAlarms810T.zip (354 Downloads) |
2/12/2011 7:45 AM | |
Posts: 259 Rating: (5) |
In initial mode i have only: DATA IN-OUT, NC DATA, PLC INITIAL, MACHINE DATA, SETUP END PW, NC ALARM. Where i can find this button that you toking about. You can see this in attachment. But the most important thing for me is how can i see inside PLC? It is possible to convert PCP backup file to STEP5 file. Or i need to somehow connect with machine using STEP5 to download PLC program. If someone know how to do that i will be grateful for help. With regards, makaveli AttachmentInitialMode.zip (371 Downloads) |
2/12/2011 10:40 AM | |
Posts: 2964 Rating: (482)
|
Hello.... You can able to see in NCMD-> Format Text memory...... does the machine is functioing or it is stopped due to this user alarm? Regards, Ekalavya |
2/13/2011 2:07 PM | |
Posts: 259 Rating: (5) |
Yes you have absolutely right and i want to do that for the beginning. But i don't have to much experience and knowledge about 810. I work mostly with new Sinumerik like 840D pl and sl. If i have this problem on 840 i would be download PLC by MPI with special converter and with Step7 ant then trace what signals logic cause alarm appears. But here i have problem because i don’t know how to download PLC program, i mean what cable i need and what is procedure for that? I download PCP file but this is only some date in hex and i cannot do nothing with it...
With regards, makaveli AttachmentPCP-PLC_PROG.zip (360 Downloads) |
2/15/2011 9:47 AM | |
Posts: 259 Rating: (5) |
Someone have any advise... With regards, makaveli |
Follow us on