10/17/2011 12:15 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Might be useful for future: Which organization blocks do you need for error handling? In case of possibility temporary to switch off (according to production, maintenance) some of existing slaves, you can use (like an option there) What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network? and Disabling DP slaves after startup of the CPU Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 10/17/2011 12:15 PM |
|
10/17/2011 12:32 PM | |
Posts: 38 Rating: (1) |
Thanks but OB 82,85,86,121,122 etc are already loaded but CPU still goes in to stop mode.Please advice. |
Last edited by: abrarfsd at: 10/17/2011 12:33 PM |
|
10/17/2011 12:34 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
As suggested above - check in diagnostic buffer the reason for that. Best regards, Hristo MIhalev |
10/18/2011 3:14 PM | |
Posts: 38 Rating: (1) |
Please see the attached file of hardware topology. The baud rate is 1.5 Mbs and the total distance is less than 100 meters. Regards AttachmentHW config.zip (209 Downloads) |
Follow us on