12/8/2015 12:57 PM | |
Joined: 9/22/2008 Last visit: 6/11/2022 Posts: 30 Rating: (3) |
Hi All I am using TP1500 Comfort panel. I have PLC UDT structure, I added structure to library (everything is ok). During the development of the faceplate I can insert PLC UDT but when I insert instance of the faceplate on the screen and try to connect value from PLC (that is with same UDT structure) error appear "Data type is not supported by the device". Also when I want to add new tag to HMI I can not select data type from library that is UDT from PLC. Is this mean that I can not use PLC UDT structure in TP1500 Comfort? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/8/2015 2:46:26 PMNew subject after splitting |
|
12/8/2015 3:41 PM | |
Joined: 9/22/2008 Last visit: 6/11/2022 Posts: 30 Rating: (3) |
Thank you for answer. I am using TIA V13 SP1 Upd5 My PLC UDT is for 1500 and I am using this connection in HMI. I know that you need to have same controller family. Please find attached screenshots with small explanation of my steps. Thanks. AttachmentTIA UDT PLC HMI problem.rar (264 Downloads) |
Follow us on