11/21/2014 6:41 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (43) |
The mlfb is not correct, i was not able to find a device with that mlfb. which step 7 version are you using? please install the newest hardware packages (HSP) then you should have the possibility to integrate the sentron in your project. you can find the latest HSPs here: http://support.automation.siemens.com/WW/view/en/23183356 http://support.automation.siemens.com/WW/view/en/72341852 |
Best Regards, |
|
11/21/2014 9:23 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
I guess, correct MLFB will be:7KM2112-0BA00-3AA0 |
This contribution was helpful to1 thankful Users |
11/21/2014 9:31 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, GSD, GSE are in the zipfile that can be downloaded here: SENTRON PAC3200 EDD for SIMATIC PDM (Process Device Manager) Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
7/24/2015 11:39 AM | |
Posts: 1 Rating: (1) |
Hello, could you help me? I need this GSD (7KM2112-0ba00-3AA0) profinet, but in the zipfile I didn´t found it. Thank you! Best regards! |
7/24/2015 12:33 PM | |
Posts: 1058 Rating: (93) |
For connecting your PAC3200 to S7 via ProfiNet you will need Switched Ethernet PROFINET Module 7KM9300-0AE01-0AA0. See here: Ethernet communication PAC3200 and PAC4200 to SIMATIC S7 7KM9300-0AE00-0AA0 - Preconditions to operate the SWTICHED ETHERNET PROFINET MODULS
Other way to communicate via Ethernet is via Modbus TCP. regards |
This contribution was helpful to3 thankful Users |
Follow us on