5/5/2008 1:14 PM | |
Joined: 5/26/2007 Last visit: 9/3/2024 Posts: 127 Rating: (3) |
am installing software redundant, after downloading i got this problem: 1. Both CPU in stop mode: - at first IM153-2 SF blink, ACT off. - at second IM153-2 every thing is OK, ACT on - SF and BF LED at both CPU are off 2. Switch CPU to RUN mode: - SF LED on at both CPU - at first IM153-2 SF blink, ACT off. - at second IM153-2 every thing is OK, ACT on Could anybody tell me what is wrong? i attach my hw config and network picture along with my program. DiagnoseA and DiagnoseB are the event i recorded from diagnose buffer of CPU A and CPU B respectively. AttachmentREDUNDANT.pdf (194 Downloads) |
5/5/2008 5:46 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
you may delete the Communication data block fromBOTH CPUS and down load the project again. if it doesnot work delete the communication Data block from the SIMATIC Manager and let the Simatic Manager create it again I have atached a PDF file for the code in OB100 you can compare between them AttachmentOB100.pdf (178 Downloads) |
Best Regards |
|
5/6/2008 11:13 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
the LADRR parameter is important if there is a communication processor else you can type the address any thing it does not matter
AttachmentFC 100 (SWR_START)_.pdf (186 Downloads) |
Best Regards |
|
Follow us on