11/24/2017 3:47 PM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 17 Rating: (0) |
Thank you for your response. Im using WinCC RT Advanced. Where can i find these limitations? |
12/24/2017 9:24 AM | |
Posts: 64 Rating: (2) |
I'm also using WinCC advanced, and I'm looking for a way to see a trend graph of an array. Is it possible? Thanks! |
2/9/2022 10:37 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello together If you are working with WinCC Professional RT then you can find some information in the WinCC V7 Manual: https://support.industry.siemens.com/cs/de/en/view/109792622/95220461067 If you are working with WInCC Comfort/Advanced then you could only work with the F(x) control to work with userdefined arrays. Theoretical you could also work with the F(t)Control but the trick is the same. you have to use a Tag log and manipulate the csv file to insert your array values. Here is an example to show the general way of this kind of workaround: https://support.industry.siemens.com/cs/ww/en/view/109481693 I hope I could calrify this kind of topics. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on