5/2/2007 6:20 PM | |
Posts: 1275 Rating: (123)
|
Sorry, but I've never used pm open export... |
5/2/2007 8:54 PM | |
Joined: 9/27/2006 Last visit: 3/20/2024 Posts: 47 Rating: (5) |
Hi, I also have never used the PM OPEN before, but you can try to register the executable application with the Windows Resource Kit tool called "srvinstw.exe". It is simple to use and the tool doesn't require installation. You can download from the link bellow or just google for it: http://www.dynawell.com/support/reskit/download/w2kinstsrv.asp |
5/3/2007 10:02 AM | |
Posts: 1084 Rating: (72)
|
I haven't used it either, but would love to hear if this is working. with regards, Ikkezelf |
5/9/2007 10:07 AM | |
Posts: 58 Rating: (1) |
It doesn't work ! When the service is started, it appears in the task manager, but 1minute more later, the service is closed and the error message appear: "The service does'nt respond to the maintenance function" Well i think that it's impossible to run a program in service when it isn't create for. Thanks to all !! Julien |
Follow us on