1/21/2012 8:44 PM | |
Posts: 6 Rating: (0) |
Hi, I get an error as shown on attachment, after I installed S7 prof 2010 SP2. Is it an solution for this?? Thanks Tony Wigdal AttachmentSImFejl.zip (1225 Downloads) |
1/23/2012 7:34 AM | |
Posts: 6 Rating: (0) |
Hi. My platform is win XP up to date, before I installed 2010 prof SP2, I had 2010 SP1. For info: I had just installed Step 7 Prof Upgrade 11. I have attached my installed software. AttachmentInstalled SIMATIC software.pdf (562 Downloads) |
This contribution was helpful to1 thankful Users |
1/23/2012 11:14 AM | |
Posts: 6 Rating: (0) |
Hi. AttachmentReadMe.zip (394 Downloads) |
3/14/2012 12:19 PM | |
Posts: 2 Rating: (0) |
Hi everybody. Did anybody get any solution from SIEMENC since the last post ? I'm affraid I have the same issue... |
Last edited by: Garam at: 3/14/2012 2:13 PM |
|
7/5/2012 8:01 PM | |
Posts: 19 Rating: (1) |
I was solved this problem with swithing off virtual net adaptor |
This contribution was helpful to1 thankful Users |
7/20/2012 2:44 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170)
|
Please guys, see following FAQ as well: http://support.automation.siemens.com/WW/view/en/61595882 |
Have Fun! |
|
This contribution was helpful to3 thankful Users |
7/31/2012 4:03 PM | |
Posts: 3 Rating: (0) |
Hey TomDeWou, thank's for your answer. You're right, on a system with WinCC i have that S7Dos component in that version you wrote, and on that system i fixed the pniopcac.exe error by changing the settings on the PNIO Dialog in PG/PC Interface Settings like discussed here:http://support.automation.siemens.com/WW/view/en/61595882. Then the pniopcac.exe errors after the ShrewSoft VPN dialup are gone. But i have different systems here without WinCC, only Simatic Manager and WinCC Flexible 2008 SP3. On that systems i cannot find S7Dos or the PNIO Dialog. Excuse my dumb question, but i'm not familiar with all the different siemens packages and their contents. What do i have to install on that kind of systems to get the S7Dos component ? Thank's ... Michael. |
Follow us on