4/28/2012 7:25 AM | |
Posts: 94 Rating: (8) |
How to calculate the no. of POs? |
4/28/2012 9:18 AM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Have you read Product Support information? How are the licenses for the AS and OS counted as from PCS 7 V7.0? And specify version of your PCS7, because it depends. Cheers. |
This contribution was helpful to1 thankful Users |
4/29/2012 8:50 AM | |
Posts: 559 Rating: (87) |
Dear Arunraje, What AMAZINGAHMED has told is 100 % true? PO can be calculated by the no of process objects which are going to use in your project. My suggestion is that if you have made I/O list then u must have P&I Diagram then u just calculate the no. of process objects from the P&I Diagram then purchase the license according. |
This contribution was helpful to1 thankful Users |
4/30/2012 11:19 AM | |
Posts: 94 Rating: (8) |
PCS7 V7.0 |
Follow us on