6/22/2011 6:44 PM | |
Posts: 15 Rating: (0) |
I have issue with WINCC asking for PO license and not using Wincc RT license which I is already supplied. 1.I have project developed in PCS7 Step 7 v 5.4 and Wincc V 6.2 When I activated the project from Wincc it is showin license missing error as attached. Wincc is asking for WINCC RT PO license but I have with me Wincc RT license. à(One soln is to convert the multiproject wincc project in to single project .Make archive and retrieve it.Then it does not ask for PO license and it takes Wincc RT tags license.I have done this for one of my project which was developed in Step 7 v 5.4 and wincc v 6.2 ..but this was NOT PCS7.)I have tried the above soln but it is still asing for PO license.Is it mandatory that since logic is developed in PCS 7,it will require PO license only?Can u provide me some solution so that I can utilize the wincc RT tags license which is being supplied and will not have to order PO license. Awaiting ur reply. I have issue with WINCC asking for PO license and not using Wincc RT license which I is already supplied. 1.I have project developed in PCS7 Step 7 v 5.4 and Wincc V 6.2 When I activated the project from Wincc it is showin license missing error as attached. Wincc is asking for WINCC RT PO license but I have with me Wincc RT license. à(One soln is to convert the multiproject wincc project in to single project .Make archive and retrieve it.Then it does not ask for PO license and it takes Wincc RT tags license.I have done this for one of my project which was developed in Step 7 v 5.4 and wincc v 6.2 ..but this was NOT PCS7.)I have tried the above soln but it is still asing for PO license.Is it mandatory that since logic is developed in PCS 7,it will require PO license only?Can u provide me some solution so that I can utilize the wincc RT tags license which is being supplied and will not have to order PO license. Awaiting ur reply. AttachmentLICENSE_po.zip (68 Downloads) |
Follow us on