2/13/2008 8:31 AM | |
Posts: 22 Rating: (0) |
Hallo DocT10000 You can use show and hide feature of WinCC Flexible, so you don't need to create faceplates. I have done a project last year with this method. In this method, you should create internal tags for every pump or motors visibility. Example: motor01_visibility_tag motor02_visibility_tag pump01_visibility_tag You are going to use these tags to show or to hide your pop up screens. There is a FAQ about this, i think it may help you better. Please write this entry ID to the search area and press enter: "23426415" or click the link below: https://support.automation.siemens.com/WW/llisapi.dll/23426415?func=ll&objId=23426416&objAction=csView&nodeid0=16502367&caller=view&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent If you have further questions, don't hesitate to ask again.. Have a nice day DerJunge |
2/14/2008 3:35 PM | |
Posts: 6 Rating: (1) |
Thx Is this the easiest way, or is there other methods we can use? Are there any dialogboxes that are already made in wincc flex? Doc |
2/28/2008 1:56 PM | |
Posts: 76 Rating: (1) |
And How do I animate this rectangle? I want to drag it |