10/6/2016 2:50 AM | |
Posts: 305 Rating: (2) |
PORTOL V14 ,does it can program with S110、S120、SIMOTION ? |
10/6/2016 4:50 AM | |
Joined: 10/2/2013 Last visit: 9/22/2024 Posts: 339 Rating: (52) |
hello Tech Wing, you should refer this link https://www.industry.siemens.com/topics/global/en/tia-portal/software/Pages/default.aspx |
Technology is best when it brings people together,so we are here now :) |
|
10/6/2016 7:28 AM | |
Posts: 305 Rating: (2) |
the V14 has not S driver ... |
10/6/2016 7:59 AM | |
Posts: 305 Rating: (2) |
1、SCOUT is has TIA and no TIA two version . after the two can up to V4.5 ? is not , D425 how can to do ? one Windows can install SCOUT V4.4 、SCOUT TIA V4.5 ? |
10/6/2016 8:16 AM | |
Posts: 305 Rating: (2) |
i have a D425 , i use it test program . new software ,i worry D425 can not to do ! |
10/6/2016 8:25 AM | |
Posts: 305 Rating: (2) |
i use SCOUT V4.4 HF11, can to test D425 . at the next time , V4.5 can not to test D425 ,wo think , i can use VMware install V4.4 to test . |
10/6/2016 8:37 AM | |
Posts: 305 Rating: (2) |
OK ,TKS . |
11/28/2016 4:58 AM | |
Posts: 305 Rating: (2) |
hello , i have a problem . PORTAL TIA V14 UDP1 witch time can download ? CUA31/32 at that time ,can in portal v14 edit ? |
Follow us on