10/30/2007 5:46 PM | |
Posts: 271 Rating: (29) |
Hello MR2, I've seldom worked with POSMO A; however, the parameter you need to change is P81. Then you need to pick the right subparameter (index). Please read through Section 4.3 in the POSMO A Configuration Manual which gives the user complete details on this transfer of data. You can do this by using FB11 or you can just simply right to the specific area in the drive. Attached is a description manual for FB10, FB11 and FB12. Hope this helps... AttachmentP7POS53b.pdf (400 Downloads) |
8/5/2008 4:57 PM | |
Posts: 1 Rating: (0) |
Hello , Could you send me FB10,FB11,FB12(Posmo A Function block for simatic S7 library),because you provided download address unable .I amchinese,so I am English not good , Didyouunderstand my means . Thank you verymuch , My e-mail 'cs5947390@126.com ' |
Follow us on