5/21/2014 9:34 PM | |
Joined: 10/10/2010 Last visit: 9/14/2024 Posts: 307 Rating: (15) |
it's a world standard which is avaliable globally ,if you need to choose the best you can try SIZER software |
5/22/2014 1:52 PM | |
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Hello Attension here I think still your question is confusing so please find the attached sheet for your reference for e.g. in the sheet there is 7.5kw & 11 kw rating VFD is available but what about between them?? Is there any special calculation for the KW Selection???? Attachmentkw rating.pdf (369 Downloads) |
Last edited by: Chetan2490 at: 5/22/2014 1:54 PM |
|
5/24/2014 11:13 AM | |
Posts: 235 Rating: (52) |
Dear sparten, we used drive to run motor, and motor is used to drive pump or other mechnical machine.Now all mechanical machine ratings are in HP.If u seen drive catalogue u will find the drive rating increase by step of 0.5HP,Now if u convert HP to KW bcox motor rating are available in KW as well as HP.and 1HP = 0.735(0.750)KW thats why u found the rating of drive or motor are .75,1.1,1.5..... For more details of HP pls find attached sheet Attachmenthorse power.pdf (332 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on