6/12/2008 9:32 AM | |
Posts: 4 Rating: (0) |
Hi All! I am glad you all likemy question. I hope somebody out there likes it as well and could point us out toa possiblesolution. |
6/12/2008 10:28 AM | |
Posts: 15 Rating: (0) |
Hi There, "Dear all, I am looking for information about components or a sort of technique that would help me to optimize the power consumption or minimize the power loses at using Sinumerik 840D on a millingmachine.Regards. H" Good starting point optimize power consumption of the Drives is to start with proper estimation of the torque you need on the axis. Due to my expericence mostly machines are over-counted. I have done more that 20 retrofits of the machines and we always use smaller motors than were orginally. Smaller motor, smaller drive, smaller infeed module. You can also apply reductors... One of the solution is to use Infeed module with feedback to net instead to resistor - during braking. |