6/22/2015 7:16 AM | |
Joined: 11/9/2008 Last visit: 4/18/2024 Posts: 402 Rating: (6) |
Thanks all of you. Yes I am using same power supply for module and CPU.So While calculating Power Consumption I don't need to consider 5V current consumption. It is already included in CPU. This last question regarding DO Module. Power consumption of DO module is not clear. DO module Doubts:-DO module is divided into 4 group and each group has its own supply like (L1+/1M; L2+/2M; L3+/3M; L4+/4M) and per group current capacity is 4 A.I have following question please help me to understand.1. I can drive 4A current per group is it right??2. This 4A current is totally depend on Load which is connected to DO. is it right ???3. While selecting Power supply or Calculating power consumption I need to consider this 4A current. is it right??Please help me to calculate proper current consumption of DO module.Regards,Yogendra G |
This contribution was helpful to1 thankful Users |
Follow us on