3/6/2013 5:28 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Hello Samir_a, there is no way to use PowerTags in PCS 7. PCS 7 is based on the PO license system. Regards |
SIMATIC PCS 7 - Overview |
|
3/7/2013 8:42 AM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating: (3) |
Dear Thunderstorm, thank you for your reply. Then I need your help with PCS7 license. Could you please be so kind and review my attached PCS7 system architecture. Here Engineering Station with installed PCS7 v8.0 upd.1 software will be used for engineering of automation systems and operator systems. This ES will also operate as Operator Station. There are also 3 Single Operator Stations on the network. Please indicate what licenses will be required there for ES and 3 OSs ? Thanks in advance. Regards, Samir
AttachmentPCS7 arch.pdf (204 Downloads) |
3/7/2013 12:58 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Hello |
SIMATIC PCS 7 - Overview |
|
3/7/2013 1:10 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
In the Siemens Industry Online Support you can find a application, in which your configuration is described. |
SIMATIC PCS 7 - Overview |
|
3/7/2013 1:23 PM | |
Posts: 836 Rating: (100)
|
You can use this config of course but I would prefer a server client solution but thats up to you. |
This contribution was helpful to2 thankful Users |
3/7/2013 4:16 PM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating: (3) |
yes, the configuration will be same as described inStandard Architectures PCS 7 V7.1 SP2, page 31 of 5.1 "Multiple OS Single System"
|
3/7/2013 5:43 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
PCS 7 V8.0 The ES license is now an ultimate license. But don`t confuse it with the AS runtime license. For download the program in the AS you need the AS RT license with the POs which your program has. Additional you need for each OS (also for your ES, which you want to use as an OS) separate OS Runtime license with the number of POs which are in the OS projct. You can see the needed number in your SIMATIC manager. If you have buy to less, it is not a problem. The licenses are countable. You can buy an additional one and the licenses POs will be added. For the AS Runtime license, you need one license with the sum of POs of your programm that you can load the program from the ES to the CPUs, it is independent of your number of CPUs. Good to know OS Runtime license: You need licens with the POs, which are direct in the OS project. |
Last edited by: Thunderstorm at: 3/8/2013 10:31 AMLast edited by: Thunderstorm at: 3/8/2013 10:13 AMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
3/11/2013 10:48 AM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating: (3) |
Thank you for help |
Last edited by: samir_a at: 4/3/2013 8:11 AM |
|
4/3/2013 11:47 AM | |
Posts: 836 Rating: (100)
|
Do you still have those 4 single stations? |
4/3/2013 12:14 PM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating: (3) |
yes, I have |
4/3/2013 1:09 PM | |
Posts: 836 Rating: (100)
|
you would need the singlestation licence and the OS PO licences for each singlstation. |
4/3/2013 2:13 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Do you have a separate engineering station with the AS/OS engineering software and license? |
SIMATIC PCS 7 - Overview |
|
4/3/2013 2:16 PM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating: (3) |
Yes, I do
|
4/3/2013 3:41 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
In your specification you have drawed 3 Single Stations, therfore you need three OS Runtime License with thenumber of POs, which are needed on the Station. |
SIMATIC PCS 7 - Overview |
|
Follow us on