2/17/2009 4:50 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello A_Taher, your CPU is a DP Master. So it is possible toconnect your CPU via Profibus. You have to import the gsd file. Here a faq about gsd files: http://support.automation.siemens.com/WW/view/en/29339779 In WinCC flexible you have to use the communication treiberSIMATIC S5 DP. regards manfred |
2/19/2009 5:56 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136)
|
Hello A_Taher, you can communicate over the adressrange with S5 driver. regards manfred |
2/19/2009 7:01 PM | |
Posts: 34 Rating: (1) |
Hello dear manfred ; I didn't get you...i hope if u can explain more in details. Thanks and best regards A_taher |
2/25/2009 10:09 AM | |
Posts: 34 Rating: (1) |
Dear Zak , Thanks for ur support,,,but i have a question ... Does the s5 driver -you mean here-act like a GSD files that can be integrated in ABB software ?? |
2/25/2009 12:13 PM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi I don't know the ABB software but if you want to configure the Profibus network you need a gsd file. Bye |
Follow us on