5/9/2018 9:33 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, You can create a simple C-action which executes at the preset times you want. Example:
Where "Print MBR Total" is your print job name You can assign a trigger to the C-action->Cyclic and define which time the action must be executed. |
Last edited by: Oreca at: 5/9/2018 10:31:24 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/9/2018 10:35 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi,
AttachmentC-script_Example_PrintJob.zip (124 Downloads) |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/9/2018 11:24 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, I hope I understand correctly what you mean. You can define in the C-action if you want to execute the action daily at 12.00u AM and 00.00PM. You can also define cycles, for example each hour or each minute and that's what you are talking about right? But if you set the cycle to "Daily", the script executes daily at 12.00AM. Another way is not to have cycles execute the action, but tags. You can define a internal tag or a tag that is compiled from your CFC program. If you connect the tag to the tag trigger (same screen), the script is executed when the tag changes from 0 to 1. That is another solution you can use... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/9/2018 11:49 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, You need to read out the tag and when the tag is "1", you execute the print job. See below example
First you define a variable in the code, then you read out the value of the tag and write it to the variable and then you check if the tag is "1" and after that, you execute the print job |
Last edited by: Oreca at: 5/9/2018 12:20:49 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/10/2018 4:37 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear moghimian, I would prefer to propose client to purchase process historian and information server. It combined with winCC seamlessly. You can generate subscription via tag trigger, message trigger or time trigger. During commissioning phase or operation phase, commissioning manager or plant manager required a lot of reports. To reduce the engineering hour and increase efficiency, information server is a good idea. Now my commissioning manager could generate whatever reports she want in a matter of minutes by herself without my help. It is too easy. You can also customize report easily and make use of Microsoft excel formula to create customized report in a short period of timeframe without the need of coding. Take a look at the siemens videos below for an overview. https://www.youtube.com/watch?v=HgnvzsYPgWA Just for your extra info. Hope it helps. |
Last edited by: Jen_Moderator at: 5/11/2018 8:04:55 AMInserted video. Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on