1/7/2008 10:26 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315) |
Hi, That is difficult, I have hat (I thought) all the problems that could happen with the CP5511, but you have find a new one... Maybe you could find a answer between the next FAQ's: How do Diagnostics and Remedy work in in STEP 7 when an online connection with the CP5511 is not possible? How can SIMATIC NET software communicate correctly with the CP 5511 in Windows 2000/XP? Checklist for using a CP5511 There are a lot of FAQ's about the CP5511, the above FAQ's are Multi-FAQ's, but there are a lot more of them when you searching on CP5511... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/9/2008 12:19 PM | |
Posts: 2 Rating: (0) |
Hello Attachmentdiag1.zip (206 Downloads) |
Follow us on