3/6/2020 10:33 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Go to C:\Program Files (x86)\SIEMENS\WinCC\uTools and open the apdiag program. Click on Output Windows and you should be getting script errors to help you identify where the problem lies. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
3/8/2020 1:44 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Well at least there are two errors in the @PG_PidConL_Standard faceplate. Please check object stUser, in there is a c-script in the dynamic property of Font and the script is used to update buttons with the correct permission. I think the faceplate is adjusted and buttons are removed or changed, but the script was not updated.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on