6/22/2009 7:12 AM | |
Posts: 557 Rating: (64) |
HI Use the industrial siemens PG for reset the MMC......... regards |
6/22/2009 3:28 PM | |
Posts: 9 Rating: (0) |
AMAZINGAHMED do you now read, I Can Connect PLC and PC. Today I make the test PROFIBUS/MPI (5512) and error is: Error 0x031a: No active PROFIBUS/MPI network found. If you want the CP of this PC to be the only active module (for example in DP master mode), the setting <PG/PC is the only master on bus> must be activated. HELLP |
6/22/2009 3:51 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Dear Zmaj, Perhaps this link might help: http://support.automation.siemens.com/WW/view/en/11492532 Best regards, Wizard |
Follow us on