Industry Online Support
Technical Forum
8/24/2012 5:01 PM | |
Joined: 1/29/2008 Last visit: 7/26/2022 Posts: 419 Rating: (19) |
Hi It means that the direction for the motor rotation is incorrect. Reverse the direction for the motor. Good luck Nit |
8/27/2012 4:35 PM | |
Posts: 2964 Rating: (478)
|
Hello, Does your Axis is with the Brake....??? brake is released... Axis Physically loaded??? 300608 says for that... check Regards, Prakash |
8/27/2012 10:32 PM | |
Posts: 5 Rating: (0) |
HI I changed the direction of motor rotation, but the alarms 25050 and 25040 are not disappeared Thanks |
8/28/2012 12:19 PM | |
Posts: 5 Rating: (0) |
HI I think the problem is in the parameters of axis or motor thanks |
Last edited by: H2H at: 8/29/2012 11:04 AMLast edited by: H2H at: 8/28/2012 12:21 PM |
|
Follow us on