2/2/2019 9:57 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
I tried simulating your exact issue and couldn't do it. At the same time I'm confident you connection problem can be resolved by as assigning an IP as per screen shots in attached file. When you are finally able to connect I would be interested in knowing how you got the red diagnostic LED to light up in PLCSIM advanced, what kind of error do you have? I can get it to flash with the CPU sill in run mode (by adding diagnostic OBs) but I couldn't get it to flash in stop. Thanks AttachmentAssignIP.zip (904 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on