12/11/2011 2:59 PM | |
Posts: 6 Rating: (0) |
Friends, Any solution to tthis problem? This is affecting my project too. |
Last edited by: O_Moderator at: 12/13/2011 11:37 AMLast edited by: O_Moderator at: 12/13/2011 11:37 AMnew subject after splitting from /tf/WW/en/Posts/12674#top |
|
12/12/2011 1:34 PM | |
Posts: 3037 Rating: (192) |
Hello, Doesthe error message appear at all projects? Do you compile with "Rebuild all"? Do you have download the image of the panel new with "Reset to factory settings"? How do you do an operating system update (OS update) on operator panels? Tweety |
12/12/2011 2:37 PM | |
Posts: 6 Rating: (0) |
I am using PCS7 v7.1 sp2. The process control servers are redundant, there are 2 Operator Stations and an engineering station. PLC is also redundant. The problem happens during both delta and ENTIRE WINCC DOWNLOAD to servers from engineering station. It doesn't happen every time but when it happens on the master server I get 'Microsoft Visual C++ Runtime Library' (i have attached the screen-shot). The server doesn't switch properly only in this scenario. I am also using WinCC tags to read from OPC Server. |
12/13/2011 2:24 PM | |
Joined: 9/29/2009 Last visit: 3/4/2020 Posts: 43 Rating: (1) |
Hi Zeesh, |
Follow us on