1/2/2008 10:02 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8740 Rating: (1168) |
Hi Genelec, When you open old project, please save and compile. Are you having any errors? Perhaps you can perform an OS update, see link: http://support.automation.siemens.com/WW/view/en/19701610 Best regards, Wizard |
1/2/2008 1:21 PM | ||
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi,
do you have the right settings in ProTool and on the OP170B? OP170B: You should look into the Transfer Settings of the OP170B. Is the serial port enabled? Link for the manual of the OP170B: (page 3-9) http://support.automation.siemens.com/WW/view/en/1838350 ProTool: Transfer Settings of ProTool: "Datei > Download > Preferences...". Is the serial port selected? Cable: Works yourserial cablecorrect? Maybe you should change your cable. Bye |
|
1/2/2008 3:17 PM | |
Posts: 22 Rating: (0) |
Hi Zak1 Yes, all setting is OK, most likely cable, I am working it out Best regards Genelec |
1/2/2008 5:51 PM | |
Posts: 22 Rating: (0) |
Hi! The cable is ok, but problem is still present Best regards |
1/3/2008 9:03 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8740 Rating: (1168) |
Hi Genelec, Well, you should deinstall the CP5511 in Device manager of Windows. Then start PC without CP5511. Please reboot PC but now with CP5511 it will automatically be recognized and installed. Also have a look at the following faq's: http://support.automation.siemens.com/WW/view/en/9853739 http://support.automation.siemens.com/WW/view/en/12259435 http://support.automation.siemens.com/WW/view/en/19279714 Hope it will help. Best regards, Wizard |
Follow us on