2/4/2020 1:03 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Well, the display of the OS server assignment looks correct. Since you are using a redundant server pair (one OS project for two servers), you only get to see one server assignment. The symbolic name of the server project entered is: SERVER2. That's just the name you have given the OS project and the name can only be given at the master server. So I guess it looks a bit misplaced, since it may seem you can only assign server 2 to the client. For the client runtime issue, that should be something else. If you have properly configured the OS servers with WinCC Application and the standby as WinCC Application (stby), and recheck all settings (see manual), it should remain connected to the other server in runtime. In the client, you must configure the standard server-> Open WinCC Explorer, right click: Server data, select Standard Server and enable the server project to: Alarms,SSM and User Archives (if you are using them). Via Server Data->Configure, you can configure the client to a preferred server, choosing server 1 or 2. but this should not be needed, because if the master server fails, the standby takes over and the client remains connected. For the faceplates... Are those custom faceplates? If yes, custom faceplate files created on the OS server project need to be copied to the client project as well.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/4/2020 8:01 PM | |
Joined: 4/18/2012 Last visit: 2/19/2024 Posts: 41 Rating: (0) |
Hi; Many thanks for your reply, According to your opinion I checked standard server configuration in client station, regrading to attached file I can only choose SERVER 2 as preferred server. As you can see in the attachment I can only configure SERVER 2 for physical and Redundant Server. I think the origination of my problem is on the SERVER 1 configuration and settings. Please see attached file no.2. As you see symbolic name Server data of OS application for SERVER 1 station selected to SERVER 2 !!! Do you think this is correct? I have another question whether we are allowed to use servers station as engineering station in PCS 7 configuration. I am using server station is also for engineering station (ES). Thank you very much in advance for your help and support AttachmentConfig.zip (276 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on