10/13/2010 7:48 AM | |
Posts: 2964 Rating: (478) |
Hello.... Power module 6SN1124-1AA00-0EA1=>160 Amps power module external cooling..... Alarm 300607 means the specified current setpoint cannot be injected in to the motor even though the maximum voltage has been provided...causemotor not connected or phase missing. Check the existing power module IGBTS by the multimeter keeping in diode range....procedure of the same is attached .... What module do you have provide me the details? Regards, Ekalavya AttachmentIGBT CHECK[1].pdf (436 Downloads) |