10/13/2021 2:44 PM | |
Joined: 3/14/2019 Last visit: 6/5/2023 Posts: 6 Rating: (0) |
Hello. I have a problem installing PCS 7 Version 8.0 SP2. I am installing this software package on a VMWare virtual machine. I install on Windows Server 2008 Stardart P2 SP1 x64, build 7601 (6.1.7601). The installer starts, when the "VC ++ 2005 SP1 Redistributable" package is installed, the error "vcredist_x86.exe" appears - Application error: The application was unable to start correctly (0x0000006). Click ok to close the application ".I click OK, the installer skips this step. Then, when installing the package "SQL Server 2008 R2 SP1 - (WinCC)", an error occurs: "NAtive SQL Install Bootstrapper". I don't know what to do, roles and features in Windows are included. I attach a photo of the Windows assembly, errors, as well as an archive with log setup Siemens/ Please, your advice is needed. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/14/2021 08:30:22New subject after splitting |
|
10/13/2021 2:48 PM | |
Joined: 3/14/2019 Last visit: 6/5/2023 Posts: 6 Rating: (0) |
AttachmentLog setup win server.zip (114 Downloads) |
10/14/2021 10:21 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Hello Dnitriy_Fenis, check the information in the FAQ: SQL Server error during installing PCS7 8.2https://support.industry.siemens.com/tf/ww/en/posts/sql-server-error-during-installing-pcs7-8-2/218192 It would help you out! |
This contribution was helpful to1 thankful Users |
Follow us on