7/14/2019 3:12 PM | |
Posts: 32 Rating: (2) |
Here is the 2nd attachment |
7/15/2019 4:39 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Ahmed_teb, Is this permanent issue? Did the system work before? Any suspicious activities before this issue happen? Can you also attached the screenshot or files for 1. Tag Archive Configuration (the next tab of your pictures, show segment settings) 2. Alarm Configuration (the next tab of your pictures, show segment settings) 3. WinCC Diagnose file (C drive - > Program Files -> Siemens -> WinCC -> Bin - > Diagnose. 4. Installed Softwares. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
7/15/2019 11:07 AM | |
Posts: 32 Rating: (2) |
Hello Jaz Tai, Thank you for your reply 1- Yes the problem is persistent and permanent 2- Yes archiving worked without any problem 3- I had a slow start-up problem of both server, and after I copy the disk image of partition C of the hard disk (I have a backup of a copy of my server) that works normal on my server current (I copy only the partition C), and after this modification I lost archiving alarms and trends. and for the wincc-> diagnose is I copying the whole file? Best regards AttachmentAlarm+tag logging.pdf (66 Downloads) |
7/15/2019 11:39 AM | |
Posts: 32 Rating: (2) |
Installed software
AttachmentInstalled software.pdf (60 Downloads) |
7/15/2019 5:09 PM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Ahmed_teb, For the WinCC Diagnose file, you can take a look into it, I'm interested in "Error" only. Can you explain more detail on item 3? I could not understand. What do you mean by copy the disk image partition C of Hard disc? A copy is not a modification, right? Slow start-up problem is related to your drive performance (SSD/HDD), RAM, Processor, the segment size you selected (Now I saw you selected 6 months for a full segment, my project normally restricted to 1 to 3 months. The rest of archive will be sent to process historian) My suggestion is, restore the original image on the problematic server. This will be an easier way. Make a backup image on the current server, restore the c drive / operating system of the server to the good one. Then set up the project again. You can solve it in no time. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
7/16/2019 4:17 PM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
That is the folder properties, read write access is very important. Glad that you found it. Thank you for sharing your solution. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on