1/29/2019 9:58 AM | |
Joined: 9/2/2013 Last visit: 2/26/2024 Posts: 128 Rating: (0) |
Dear All, Kindly assist me with below problem. My problem is doing delta download (Changes only) from Engineering workstation to the OS servers. I get the attached file error and asking me to do entire download.
I also getting from error message of "OSSVR B: No access to SQL Server, Data Loss Possible". When this error message keeps popping up I re started Server B to rectify it. Any suggestion will be highly appreciated. Regards, Attachmentos_dOWNLOAD_lOG.zip (85 Downloads) |
1/30/2019 3:34 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Dear PCS 7 , i assume you cannot do an OS entire download in your standby server right? Have you success download before? any previous load log? May be you can take a look at the diagnose folder. C:\Program Files (x86)\SIEMENS\WINCC\diagnose Sort the latest date , see any useful log files giving you a hints or not. Hope it is helpful |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/31/2019 10:58 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Dear PCS 7, When I have an issue with SQL, normally I will do a few things, 1. check the PCS 7 OS folder in the target folder, add a window login user into the folder. For example, you are using USER1 as logon for ES and OS B, then I will add USER1 to the security of the folder. (although the USER1 has been given roles like administrators and SIMATIC HMI Group and the folder has these groups right) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on