6/4/2011 7:16 AM | |
Posts: 10 Rating: (0) |
hai everybody i am using s7 300 software redundant program...... cpu 315 2 dp with 3 remote station during operation power failure at any remote station cpu (master) switching to cpu (slave).. i want to avoid master to slave change over during dp slave power fail condition.. i got one sample program from simens manual... but if i enter that program it showing error.. i wriiten that example logic in OB 86 i cant able to use that program... can you send the actual program for this application.. i attached the manual & program page for your reference Attachmentredundant problem.pdf (58 Downloads) |
6/4/2011 11:06 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi sraj, page 502 OB info, have you check from PLC diagnostic is there other problems? http://support.automation.siemens.com/WW/view/en/45531107 regards Heksu for communication
|
Last edited by: Heksu at: 6/4/2011 11:07 AM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
6/5/2011 7:14 AM | |
Posts: 10 Rating: (0) |
hai hesku.. i want to AVOID the master to slave change over during rack failure sitiuation... for that i seen one sample program in manual.. i can' t able use that program in my logic because if i enter that logic codes are become red colour for example "SPBN M001" & "AUF" these codes are used in logic... now i hope you will understand my requirement...if possible send me the actual program for that... thanks Attachmentrack failure error.pdf (33 Downloads) |
6/5/2011 8:44 AM | |
Joined: 10/7/2005 Last visit: 5/8/2024 Posts: 3004 Rating: (1046)
|
Hello it seems Siemens "forgot" to translate the example program from German mnemonics into English ones. There's two ways to fix this: 1.) change your Step 7 to Germanmnemonics (Options menu->Customise->Language tab), entertheexample program into your OB86 and then change Step 7 back to English mnemonics. 2.) Use the following English mnemonics based commands in place of the German ones: SPBN--> JCN U --> A AUF--> OPN I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on