9/17/2008 10:31 AM | |
Posts: 1776 Rating: (95)
|
Hi, the reason is that some programs are started in Windows services automatically |
9/1/2013 7:34 PM | |
Posts: 16 Rating: (0) |
Dear all, |
9/2/2013 9:24 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
1. Stop the WinCC server in SQL enterprise manager 2. Archive 3. Enable server Or Reset_wincc.vbs under the command prompt under Start windows |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
9/3/2013 10:43 AM | |
Posts: 836 Rating: (99)
|
Hi, check out the steps I described in this topic. If it is not working, get back in touch with me, there might be another solution. |
Follow us on