Industry Online Support
Technical Forum
11/3/2011 11:39 AM | |
Posts: 7 Rating: (1) |
Hello, I'v encountered the following problem:PG is connected to CPU315-2 PN/DP via Ethernet.The CPU315-2 PN/DP is connected to Sinamics S120 with CU320 via Profibus.When I'v tried to connect Scout to do some changes to inverter, connection could not be established.I could download the HW configuration and NetPro configuration to the CPU, and there is not fault on BF. The hardware: CPU 315-2 PN/DP 6ES7315-2EH13-0AB0 V2.5 CU320: 6SL3040-0MA00-0AA1 CF card: 6SL3054-0CE01-1AA0 performance 1 V2.4.1.6 The Software: Step 7 V5.5 Scout: V4.2. sp1 AttachmentScreenshots.pdf (156 Downloads) |
11/7/2011 4:20 PM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating: (17) |
Hello, This should be a problem with SIMATIC CPU. Please post this problem to the SIMATIC forum. Regards Manfred |
Follow us on