6/2/2020 11:16 AM | |
Posts: 2 Rating: (0) |
We have a windows server 2003 that is running a PC station that is hosting an OPC Server. This server is outdated and we want to move things over to windows 2019 server. I tried to import the XDB file on the new server but this fails because it doesn't the IP address differs from the one configured in the XDB. We don't have the project anymore, so I created a new one. But I can't seemed to get data from the PLC. https://trackeasy.fun/usps/ https://showbox.tools/ http://essaywriter.fun/ In Simatic Manager I created a new project and added a SIMATIC PC Station. I added an OPC server and IE General (see attach1.jpg) I configured the IE General component to use the IP address of the new server. On the OPC server I added a S7 connection. (see attachment) I saved the project and used the generated XDB file to setup the PC Station. When I connect using OPC scout, I don't see the same addresses that are available when I connect to the old opc server. |
Last edited by: AdonisReed at: 06/04/2020 09:14:26Last edited by: AdonisReed at: 06/04/2020 09:15:11 |
|
6/4/2020 1:42 PM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 7998 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Problem setting up PC Station: OPC Server is published within the conference Communication / Networks. Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on