6/27/2019 9:55 PM | |
Joined: 10/10/2017 Last visit: 7/21/2024 Posts: 61 Rating: (0) |
I have a problem to connect to D435, I did everything according to the Simotion Getting Started and yet I can not connect. The error message I get is "The attempt to establish a connection to an incompatible device". The initial Ethernet address of the Simotion Device is 169.254.11.22 and I set the address of my PC to be 169.254.11.99 as given in the Getting started manual, and after I select the hardware and try to connect the error message pops out. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/28/2019 10:08:20New subject after splitting |
|
6/28/2019 6:14 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
hello, please add a screen of all messages ! i think you have different FW Version offline/Online.
Christoph |
6/28/2019 9:46 AM | |
Joined: 10/10/2017 Last visit: 7/21/2024 Posts: 61 Rating: (0) |
Here is the picture of all errors. |
6/28/2019 10:24 AM | |
Joined: 10/10/2017 Last visit: 7/21/2024 Posts: 61 Rating: (0) |
The version of the D435 in the software is V4.4. And CF card inserted in the CU is V5.1 HF1. |
6/28/2019 10:54 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hi, this versions are not compatible. For Version V5.1 on the Target you need Scout V5.1 or above.
Christoph |
Follow us on