3/2/2016 10:59 AM | |
Joined: 4/10/2009 Last visit: 10/23/2023 Posts: 94 Rating: (0) |
Dear Christoper I have the similar problem to connect to Simotion. I did the following 1. Enable IP router in Remote PC. Restarted the remote PC 2. Reconfirmed the enable by ipconfig/all comment in command prompt in both remote PC and programmer PC 3. The remote Simotion IP address is 192.168.2.1 and TV ID is 7.183.228.202 4. Then did the Route add 192.168.2.1 mask 255.255.255.0 7.183.228.202 metric 1. Got OK after entering. 5. Then in PG/PC Interface choosen TV adapter for communication. But still I am not able to connect to Simotion. Kindly suggest where I am missing? Regards Prian ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/3/2016 10:36:09 AMNew subject after splitting |
|
3/7/2016 10:26 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Htet Aung is split to a separate thread with the subject Bus Fault:Missing Slave in Simotion, what I have to check?. Best regards |
Follow us on