10/10/2019 4:05 PM | |
Joined: 11/24/2015 Last visit: 1/8/2023 Posts: 14 Rating:
|
Hi i have a Problem to install Maria DB on IOT2020 System: IOT2020 SD-Image 2.4 We tried the PDF."Install SQL server on IOT2000 on two IOT2020" without USB Media Our Problem is Step 9. "Start installation script for MariaDB ./scripts/mysql_install_db --datadir=/media/storage/sqldb Our Result is this message "Neither host 'iot2000' nor 'localhost' could be looked up with './bin/resolveip' Please configure the 'hostname' command to return a correct hostname. If you want to solve this at a later stage, restart this script with the --force option" hostname"iot2000" /etc/hosts "127.0.0.1 localhost.localdomain localhost # The following lines are desirable for IPv6 capable hosts ::1 localhost ip6-localhost ip6-loopback fe00::0 ip6-localnet ff00::0 ip6-mcastprefix ff02::1 ip6-allnodes ff02::2 ip6-allrouters" we tried with mariadb-5.5.65-linux-i686 and mariadb-10.3.13-linux-i686 we have no Internet access on the LAN, we use if needed USB Dongle with Cellphone Accesspoint where is my Problem?? hope someone can help me/us
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/10/2019 17:19:14New subject after splitting |
|
Follow us on