6/6/2014 2:40 PM | |
Joined: 3/28/2014 Last visit: 9/5/2024 Posts: 82 Rating: (0) |
thanks a lot I agree all thay you say. I hope Im not bore, and disturbing you. I ve learned a lot in this case and as I can take this conclusion: 1.%TEA 1 file contains the machine data sholud be put at NC *this file I miss so is it possible to start PLC without file??? 2.%TEA2 file contains the machine data sholud be put at PLC 3.%PCP -PLC program 4.%PCA - NC Alarms explanation. Without this file the CNC will work giving alarms but there will be not explanation after Alarm number. In attacment are alarms at CNC. The main problem is that PLC is in STOP mode- not working. Thanks for help
Attachment820 Alarms.pdf (514 Downloads) |
6/8/2014 4:11 PM | |
Joined: 3/28/2014 Last visit: 9/5/2024 Posts: 82 Rating: (0) |
So At the end I didnt find solution yet but I have concrete conclutoins: If I want to make backup i will take the following files: 1.NC MD => % TEA1 the file Im still missing. without this file I get allarm nr. 11 wrong UMS identifier. Still I dont know wht exactly to do because I dont understand explanations. If I clear nc system bit 5015.6 then the allarm wil dissapear. I dont know is it right ??? 2.PLC MD=>%TEA2 3.PLC PRG=>%PCP *EMPTY* After battery failrue. If I Put PCP file from FDD => Sinumerik(PLC) then I will get alarm message nr 3 PLC STOP mode. 4.UMS DAT=>%ASM the think that confusing me most!!! I ve tried to put ASM file contained in the backup floppy disk in Initial clear mode and in normal data input/ output mode withot results. I dont understand that because if You take backup file from Sinumerik normally is that file could be downloaded in Sinumerik to restore machine So please anyone can help me with any information I will be gratefull. At the attachment are files I downoaded from sinumerik to my PC. Thanks AttachmentMY Sinumerik backup.zip (597 Downloads) |
This contribution was helpful to1 thankful Users |
6/17/2014 6:29 AM | |
Joined: 3/28/2014 Last visit: 9/5/2024 Posts: 82 Rating: (0) |
hello one more time I'm asking all members willing to help to me about my CNC Sinumerik 820 to explai to me what is meaning(function) of UMS. Exactly I'm able to make backup of UMS but I dont know what with this file? Is it possible lost %TEA1 file to take from UMS in attachment??? It is impossible to download to my sinumerik !!! And another quetion what I need to do to make "Load plcprogram" steakers appear at initial clear mode. Thanks in advance
Attachment820 Data output.pdf (484 Downloads) |
Follow us on