10/19/2020 2:45 PM | |
Joined: 7/26/2011 Last visit: 4/8/2024 Posts: 11 Rating: (0) |
Hi all! I have a problem using SFC51 for PN diagnostics on a pair of redundant CPU 410-4H. I use SSL-ID # 0294 (Actual status of the rack in the central rack / stations of an IO controller system for PNIO) and my data receiving DB contains 1 WORD index and 2048 status BOOL as indicated in the manual. When the master CPU is in SOLO-MODE the SFC51 works, but as I try to synchronize the CPUs they both go to stop and I don't understand the cause. - function # 0294 can be used with CPU-Hs? - need to extend the size of the DB DataRecord? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/20/2020 07:40:35New subject after splitting |
|
Follow us on